About this task
The Relearn feature uses Auto Discovery and requires that the supervisory controller be online with the BACnet network to discover Field Devices and Field Points.
Procedure
- Select the BACnet Integration object from the Navigation tree.
- Click the Engineering tab and click the Relearn button that appears below the tab.
- Discovery begins automatically and finds all new BACnet devices on the network. After Discovery, the new devices appear in the Integration Tree and in the Integration View.
- When Discovery is complete, close the Auto Discovery box.