About this task
The following process is applicable to online configuration in the Site Management Portal UI or offline configuration in the SCT. These procedures assume both an online configuration and a connection between the NAE and the same network as the BACnet system or the integrating devices.
The SCT contains no Engineering or Diagnostics views, as these are online features. In addition, to use Auto Discovery, the system must be online and connected to a BACnet network of devices.
Note: At startup of the supervisory
controller, the BACnet Integration binds with the BACnet OID and uses the IP address
from that bind. If you move a device to a different subnet, change the IP address of
the device, or change the device's BACnet OID, you must restart the supervisory
controller to bind the BACnet OID with the new IP address.