Supported network engine objects - Metasys - LIT-1201531 - System Integration - BACnet Controller Integration - 10.1

BACnet Controller Integration Technical Bulletin

Product
Controls > BACnet Controls > BACnet Controller Integration
Document type
Technical Bulletin
Document number
LIT-1201531
Version
10.1
Revision date
2021-10-08
Note: The M-Series Workstation Interface to the network engine supports access to the network engine objects listed in the following table, with the exception of the Averaging object extension.
Table 1. Supported supervisory controller objects

Analog Value (AV)

Binary Output 1

Binary Value (BV)

Multistate Input1

Event Enrollment (EEO)

Multistate Output1

Interlock

Notification Class

Multiple Command

Accumulator object

Analog Input1

Trend Log object extension 2

Analog Output1

Totalization object extension2

Binary Input1

Averaging object extension2

Objects from the following devices are not available to the M-Series Workstation:

  • NIE55

  • ADS

  • ADX

  • ODS

  • OAS

1 With N2 or LonWorks Hardware Tab (points can be interfaced from N2 devices as well as LonWorks devices).
2 Object extensions appear as a separate object within third-party BACnet devices.