Configuring a Network Engine as a BACnet/IP to MS/TP Router - Metasys - LIT-1201531 - System Integration - BACnet Controller Integration - 10.1

BACnet Controller Integration Technical Bulletin

Product
Controls > BACnet Controls > BACnet Controller Integration
Document number
LIT-1201531
Version
10.1
Revision date
2021-10-08
In its default configuration, third-party BACnet/IP devices can only see the integrated BACnet objects of the network engine. If the BACnet Routing mode is set to Enabled in the network engine, then other BACnet devices on the IP network are able to communicate directly with BACnet MS/TP devices. See Enabling the routing mode.
Note: In most cases, enabling routing is not recommended.