Unique device object identifiers - Metasys - LIT-1201531 - System Integration - BACnet Controller Integration - 10.1

BACnet Controller Integration Technical Bulletin

Product
Controls > BACnet Controls > BACnet Controller Integration
Document type
Technical Bulletin
Document number
LIT-1201531
Version
10.1
Revision date
2021-10-08

Each BACnet device object at a site must have a unique instance number and name. The BACnet device object instance number and name are assigned in the field as part of the installation configuration. When assigning instance numbers and names to device objects at a site, we recommend maintaining a list of devices and their assigned BACnet device object unique instance numbers and names.