Ordering information - Metasys - LIT-1901143 - M4-ADSTK-PC - M4-ADXTK-RCK - M4-ADXTK-TWR - ADS/ADX Turnkey - 13.0

Application and Data Server (ADS/ADX) Turnkey Computer Systems Catalog Page

Product
Building Automation Systems > Application Servers > ADS/ADX Turnkey
Document type
Catalog Page
Document number
LIT-1901143
Version
13.0
Revision date
2023-10-25
Product status
Active

Order both hardware and software licenses when you purchase a Turnkey system. See Table 1 for available hardware options, and Table 2 for software licenses. For complete software ordering information, refer to the Metasys System Software Purchase Options Product Bulletin (LIT-12011703).

Important: For an ADX Turnkey system, you require a license for Microsoft SQL Server 2022. For product codes that include both Microsoft SQL Server 2022 and Metasys ADX software licenses, see Table 2. These product codes use core-based licensing for SQL Server and include a license for 4 cores. You must ensure that you adequately license Microsoft SQL Server for the number of cores listed in the technical specifications. In the per-core licensing model, licenses are sold as 2 core packs. If you purchase a 4 core license from Johnson Controls, then you must separately purchase an additional two 2 core license packs for the M4-ADXTK-TWR or an additional six 2 core license packs for the M4-ADXTK-RCK. For more information about purchasing licenses, refer to the License requirements for servers and SQL Server section in the ADS/ADX Commissioning Guide (LIT-1201645).
Note: If you obtain an SQL Server license from somewhere other than Johnson Controls, you can choose between core-based and Server + CAL licensing models. Compare both to determine the most cost-effective option, but also consider possible future expansion.

You must also purchase a Windows Server CAL for each client or device that accesses an ADX Turnkey. These are required to connect to the Microsoft Server OS, and are independent of any CALs that you purchase to license Microsoft SQL Server through a Server + CAL licensing model. For examples of Windows Server CAL purchases, see Table 3. For information about choosing between user and device CALs, and how to purchase CALs, refer to the Microsoft Windows operating system and SQL Server software license requirements appendix in the ADS/ADX Commissioning Guide (LIT-1201645).

Important: ADS/ADX Turnkeys are not suitable for large sites or many users, such as for customers that require 50-user or 100-user licenses. For the specifications of appropriate hardware, refer to the Application and Data Server (ADS) and Extended Application and Data Server (ADX) Catalog Page (LIT-1900200).
Table 1. ADS/ADX Turnkey hardware ordering information
Product code Product description
M4-ADSTK-PC

Dell OptiPlex XE4 small form factor industrial grade desktop

Installed: Microsoft Windows 10 Pro, Microsoft Defender Antivirus enabled, Microsoft SQL Server 2022 Express, unlicensed Metasys ADS Release 13.0 software, unlicensed Fault Detection software, unlicensed Fault Triage software, unlicensed SCT Release 16.x software and required device packages

Additional requirements: Metasys ADS license. You do not require a license for SQL Server or Windows Server CALs.

Optional: See additional software listed in Table 2

M4-ADXTK-TWR

Dell PowerEdge T550 rack-mountable tower server

Installed: Microsoft Windows Server 2019, Microsoft Defender Antivirus enabled, unlicensed Microsoft SQL Server 2022, unlicensed Metasys ADX Release 13.0 software, unlicensed Fault Detection software, unlicensed Fault Triage software, unlicensed SCT Release 16.x software and required device packages

Additional requirements: Metasys ADX license, Microsoft SQL Server 2022 license, Windows Server CALs

Optional: See additional software listed in Table 2

M4-ADXTK-RCK

Dell PowerEdge R450 rack server

Installed: Microsoft Windows Server 2019, Microsoft Defender Antivirus enabled, unlicensed Microsoft SQL Server 2022, unlicensed Metasys ADX Release 13.0 software, unlicensed Fault Detection software, unlicensed Fault Triage software, unlicensed SCT Release 16.x software and required device packages

Additional requirements: Metasys ADX license, Microsoft SQL Server 2022 license, Windows Server CALs, server rails

Optional: See additional software listed in Table 2

Table 2. Metasys software ordering information and Turnkey hardware compatibility
Product code Description M4-ADSTK-PC M4-ADXTK-TWR M4-ADXTK-RCK
MS-ADS05U-0 ADS 5-user license - -
MS-ADX10U-0 ADX 10-user license -
MS-ADX10SQL ADX 10-user and Microsoft SQL Server license for 4 cores -
MS-ADX25U-0 ADX 25-user license -
MS-ADX25SQL ADX 25-user and Microsoft SQL Server license for 4 cores -
M4-FAULT-0 License enabling the Fault Detection feature for one Metasys server
M4-TRIAGE-0 License enabling the Fault Triage feature for one Metasys server
Note: M4-FAULT-0 is also required as a prerequisite.
M4-ADFS-0 License enabling the Active Directory Federation Services
M4-FIPS-0 License enabling Federal Information Processing Standard 140-2 (FIPS 140-2 Level 1 compliance)
M4-APIMOCMD-0 License enabling the Monitoring and Commanding API
M4-APIMOCMD-6 License enabling the upgrade of the Monitoring and Commanding API for existing sites
Note: Existing sites upgrading to Release 12.0 or later must purchase this upgrade to continue using the API.
TL-SCT-0 System Configuration Tool (SCT), one user license
MS-FCP-0 License enabling Metasys brand field controller package files
MS-DP-0 License enabling Metasys device packages
TL-BUNDLEMS-0 Tool Bundle Metasys, includes TL-SCT-P, which provides access to both the 14.x and 13.x versions of SCT
M4-BACNETSC-0 License enabling BACnet Secure Connect
Important: SCT 14.1 and later requires that you activate MS-FCP-0 and MS-DP-0. Turnkeys ship with both device packages preinstalled but unlicensed. Licensing these two device packages, a new requirement at SCT 14.1, allows you to add controllers to an SCT archive.
Note: Turnkeys include additional software that is bundled with the ADS/ADX server software, including the Metasys UI and the Metasys Database Manager. For further information about included and optional software that relate to an ADS or ADX server, refer to the Application and Data Server (ADS) and Extended Application and Data Server (ADX) Catalog Page (LIT-1900200).
Table 3. ADX License and CAL Examples
ADX Offering Example number of Windows Server CALs Example mix of user and device CALs
ADX 10-user 5

5 CALs = 2 user CALs + 3 device CALs

5 CALs = 3 user CALs + 2 device CALs

10

15 CALs = 10 user CALs + 5 device CALs

15 CALs = 8 user CALs + 7 device CALs

ADX 25-user 30

30 CALs = 25 user CALs + 5 device CALs

30 CALs = 10 user CALs + 20 device CALs

The ADX Turnkey computers come in two varieties: tower and rack. Use the tower hardware option for flexibility in installation, and the rack hardware option to conserve space in a server rack.