Applications - Metasys - LIT-1901143 - M4-ADSTK-PC - M4-ADXTK-RCK - M4-ADXTK-TWR - ADS/ADX Turnkey - 13.0

Application and Data Server (ADS/ADX) Turnkey Computer Systems Catalog Page

Product
Building Automation Systems > Application Servers > ADS/ADX Turnkey
Document type
Catalog Page
Document number
LIT-1901143
Version
13.0
Revision date
2023-10-25
Product status
Active

Use a Turnkey system to simplify new installations of an ADS or ADX to accompany a new or existing installation of Metasys at Release 12.0 or later. For information about when to choose an ADS or ADX, refer to the Application and Data Server (ADS) and Extended Application and Data Server (ADX) Catalog Page (LIT-1900200) .

The ADX Turnkey computers come in two varieties: Tower and Rack. Use the tower hardware option for flexibility in installation, and the rack hardware option to conserve space in a server rack.