Extended Application and Data Server (ADX) - Metasys - LIT-1201525 - MS-ADS05U - MS-ADX10SQL - MS-ADX10U - MS-ADX25SQL - MS-ADX50SQL2 - MS-ADX50U - MS-ADXS25U - Server - ADS Server - ADX Server - 14.0

Application and Data Server (ADS) and Extended Application and Data Server (ADX) Product Bulletin

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document type
Product Bulletin
Document number
LIT-1201525
Version
14.0
Revision date
2024-12-09
Product status
Active
The ADX provides more advanced historical data management. The ADX supports up to 10, 25, 50, or 100 concurrent users connected through a combination of the Metasys UI (maximum 50 users) and the Site Management Portal UI. The ADX offers manual, automatic, and scheduled archiving of historical data and offers extended reporting capabilities using SQL Server software or third-party software. For more information about supported concurrent users, refer to the ADS/ADX concurrent users section in the Metasys System Configuration Guide (LIT-12011832).
Note: SMP requires a license that is available to existing Metasys customers only.

The ADX may be installed in a split configuration. Splitting provides enhanced security for historical data. The ADX software and user interface are installed on one computer known as the web/application server computer, and the historical trend, audit, and event data on another computer, the database server computer that runs Microsoft SQL Server software.