|
Characteristic |
ADS |
ADX |
Questions to Ask |
|---|---|---|---|
|
Database Capacity 1 |
10 GB |
40 GB (minimum free space required on the computer after ADX installation) The database can expand until all hard disk space is used. |
|
|
Archive Type Available |
Manual |
|
Do you need automatic or scheduled archiving?
|
|
Archiving Tools |
|
|
Do you have experienced Information Technology specialists on hand? If you have experienced IT specialists on site, they may require specific third-party archive management tools or prefer the powerful SQL Server software capabilities of the ADX. |
|
Site Management Portal UI System Configuration Tool (SCT) System Configuration Tool Pro (SCT Pro) |
Metasys UI Johnson Controls System Configuration Tool (JCT) |
|
|---|---|---|
|
Recommended processor 4 |
Intel® Core™ i5 Processor |
Intel® Core™ i5 Processor |
|
Recommended Random Access Memory (RAM) |
32 GB |
32 GB |
|
Note: If you use graphics intensively, you may
experience better computer performance with additional
RAM.
|
||
|
Hard disk capacity |
40 GB hard disk (minimum) |
40 GB hard disk (minimum) |
|
Supported operating systems |
SMP Windows® 11 Pro and Enterprise (23H2, 22H2) Windows® 10 Pro and Windows 10 Enterprise Editions version 22H2 (64-bit). For all future Windows 10 updates after version 22H2, we will evaluate and certify that Metasys software can support the updates before we provide guidance on support. Windows® 10 Enterprise and IoT Enterprise LTSC (1809, 21H2 ) SCT and SCT Pro Windows® 11 Pro and Enterprise (23H2, 22H2) Windows® 10 Pro and Windows 10 Enterprise Editions version 22H2. Windows® 10 Enterprise and IoT Enterprise LTSC (1809, 21H2 ) Windows® Server® 2022 Windows® Server® 2019 version 1809 or later (64-bit) |
Metasys UI and Johnson Controls System Configuration Tool (JCT) Windows® 11 Pro and Enterprise (23H2, 22H2) Windows® 10 Pro and Windows 10 Enterprise Editions version 22H2 (64-bit). For all future Windows 10 updates after version 22H2, we will evaluate and certify that Metasys software can support the updates before we provide guidance on support. Windows® 10 Enterprise and IoT Enterprise LTSC (1809, 21H2 ) Apple® macOS® 10.15 Catalina Apple® macOS® 10.14 Mojave Apple® macOS® 14 Sonoma |
|
Supported web browsers |
Google® Chrome™ version 124 or later Microsoft® Edge® version 124 or later
Apple®
Safari®
16.1
Note: In macOS, you cannot view Graphics+
graphics in the Site Management Portal UI. You use the web
browser to download the Launcher application. After you
install the Launcher application, you use the Launcher, not
the web browser, to log in to the Site Management Portal
(SMP) UI.
|
Microsoft® Edge® version 124 or later
Google®
Chrome™ version 124 or later
Note: Metasys UI
does not support Incognito mode. To exit Incognito mode,
click or tap the X icon of the browser window or tab
and then open a new browser window or tab. For more
information on Incognito mode in Google Chrome, click here.
Apple®
Safari®
16.1 or later
Note: Metasys UI does not support private
browsing. To exit private browsing, click or tap
Private in the browser window.
Other web browsers, such as Mozilla® Firefox®, are not officially supported by the UI. However, the Metasys UI may appear and function appropriately in these web browsers. |
|
Supported mobile phone operating systems |
N/A |
Android phone 11.0 or later iPhone iOS 13.0 or later |
|
Supported tablet operating systems |
N/A |
Android tablet 11.0 or later iPad iOS 13.0 or later |
|
Network communication |
Ethernet network interface card 10/100/1000 Mbps |
Ethernet network interface card 10/100/1000 Mbps Follow these guidelines and recommendations:
|
|
Monitor |
1024 x 768 or higher resolution and 16-bit or higher color depth |
1024 x 768 or higher resolution and 16-bit or higher color depth. Designed for 1920 x 1080 resolution. Other features may require 1600 x 900 resolution. Additionally, you may need to set your monitor display at Small 100% setting (Control Panel > All Control Panel Items > Display). |