Site Management Portal UI - Metasys - LIT-1201525 - MS-ADX50SQL2 - MS-ADX25SQL - MS-ADXS25U - MS-ADS05U - MS-ADX10SQL - MS-ADX10U - MS-ADX50U - Server - ADS Server - ADX Server - 13.0.50

Application and Data Server (ADS) and Extended Application and Data Server (ADX) Product Bulletin

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document type
Product Bulletin
Document number
LIT-1201525
Version
13.0.50
Revision date
2024-01-23
Product status
Active

The Site Management Portal UI provides system administrators or building operators online user and system configuration capabilities along with real-time views into their site. The Site Management Portal UI transforms raw data from the site and organizes it into a comprehensive set of information management tools and reports.

The Site Management Portal UI framework features a multiple panel layout that displays different aspects of your building control system at one time. For example, you can display a graphic diagram of an air handling plant along with a multiple point trend graph and the control system logic. This multi-panel layout allows you to identify the cause of an alarm condition from the plant quickly. In another panel, you can display a detailed focus view of a point and monitor the effects of changes to its value on the system graphic in the other panel.