Metasys for Validated Environments (MVE) - Metasys - LIT-1201525 - MS-ADX50SQL2 - MS-ADX25SQL - MS-ADXS25U - MS-ADS05U - MS-ADX10SQL - MS-ADX10U - MS-ADX50U - Server - ADS Server - ADX Server - 13.0.50

Application and Data Server (ADS) and Extended Application and Data Server (ADX) Product Bulletin

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201525
Version
13.0.50
Revision date
2024-01-23
Product status
Active

Metasys for Validated Environments (MVE) is an offering for facilities that require regulatory compliance for their environmental systems. MVE brings the flexibility and convenience of a web interface to your regulated facility. An MVE site consists of a validated MVE site director (ADX) plus one or more validated child engines. An MVE site can optionally include non-validated engines. On an MVE site, the validated ADX site director and its validated engines are both types of validated devices. For information about supported engine models, refer to the Metasys for Validated Environments on Metasys UI Technical Bulletin (LIT-12014262). At release 13.0.50, an ADX with MVE provides both MVE on SMP UI and MVE on Metasys UI. The MVE application is ordered separately from the Metasys Extended Application and Data Server (ADX).

For information about MVE on Metasys UI, refer to the Metasys UI Help (LIT-12011953). For information about MVE on SMP UI, refer to the Metasys Site Management Portal Help (LIT-1201793).

Note: On an MVE site, Metasys UI dashboards, widgets, and features may be different than described in later sections. For details of any differences, see the Metasys for Validated Environments section of the Metasys UI Help (LIT-12011953).