Fault Detection and Fault Triage - Metasys - LIT-1201525 - MS-ADX50SQL2 - MS-ADX25SQL - MS-ADXS25U - MS-ADS05U - MS-ADX10SQL - MS-ADX10U - MS-ADX50U - Server - ADS Server - ADX Server - 12.0.50

Application and Data Server (ADS) and Extended Application and Data Server (ADX) Product Bulletin

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document type
Product Bulletin
Document number
LIT-1201525
Version
12.0.50
Revision date
2023-05-22
Product status
Active
Fault Detection
  • Fault Detection is a licensed add-on feature to the Metasys Server software products, including ADS, ADX, ADS-Lite, and OAS.
    Note: At a minimum, you require 8 GB of RAM and four virtual cores to support the Fault Detection and Fault Triage features on an OAS.
  • This feature identifies building system-related faults and lists them in order of severity, whereby it leverages Johnson Controls-defined rules and a semantic data model to ease configuration.
  • Fault Detection helps operators identify issues of building systems that are not operating correctly, prevent energy waste, and avoid comfort complaints. The feature is delivered in a way that minimizes configuration workflows.
Fault Triage
  • Fault Triage is a licensed add-on feature to Fault Detection and the Metasys Server software products, including ADS, ADX, ADS-Lite, and OAS.
    Note: At a minimum, you require 8 GB of RAM and four virtual cores to support the Fault Detection and Fault Triage features on an OAS.
  • Fault Triage improves the fault list order by adding fault duration and occurrence to the sorting logic, which improves driving the biggest problems to the top of the list.
  • Fault Triage leverages the Johnson Controls Field Support Knowledge Database to suggest possible causes, their likelihood, and appropriate corrective actions.
  • The feature captures corrective action activity that includes not tried, tried, and solved issues with the ability to add notes.
  • In addition, Fault Triage offers automatically generated, multi-stacked charting of fault data for each fault occurrence.
  • Fault Triage provides an assisted experience for less experienced HVAC controls technicians.
Note: No significant feature additions were made to Fault Detection and Fault Triage at Release 12.0. The Metasys Fault Detection license and Metasys Fault Triage license remain at 11.x and continue to work at 12.x.

The functionalities of Fault Triage and Fault Detection are documented in detail in the Potential Problem Areas widget section of Metasys UI Help (LIT-12011953) .