|
Characteristic |
ADS |
ADX |
Questions to Ask |
|---|---|---|---|
|
Database Capacity 1 |
10 GB |
40 GB (minimum free space required on the computer after ADX installation) The database can expand until all hard disk space is used. |
|
|
Archive Type Available |
Manual |
|
Do you need automatic or scheduled archiving?
|
|
Archiving Tools |
|
|
Do you have experienced Information Technology specialists on hand? If you have experienced IT specialists on site, they may require specific third-party archive management tools or prefer the powerful SQL Server software capabilities of the ADX. |
|
Site Management Portal UI System Configuration Tool (SCT) System Configuration Tool Pro (SCT Pro) |
Metasys UI Johnson Controls System Configuration Tool (JCT) |
|
|---|---|---|
|
Recommended processor 4 |
Intel® Core™ i5 Processor |
Intel® Core™ i5 Processor |
|
Recommended Random Access Memory (RAM) |
8 GB (4 GB minimum) |
8 GB (1 GB minimum) |
|
Note: If you use graphics intensively, you may
experience better computer performance with additional
RAM.
|
||
|
Hard disk capacity |
40 GB hard disk (minimum) |
40 GB hard disk (minimum) |
|
Supported operating systems |
SMP Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H1 and 21H2 For all future Windows 10 updates after version 2004, we will evaluate and certify that Metasys software can support the updates before we provide guidance on support. SCT and SCT Pro Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H1 and 21H2. Windows® Server® 2019 (version 1809 or later) (64-bit) Windows® Server® 2016 (version 1607 or later) (64-bit) |
Metasys UI and Johnson Controls System Configuration Tool (JCT) Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H1 and 21H2 (64-bit). For all future Windows 10 updates after version 2004, we will evaluate and certify that Metasys software can support the updates before we provide guidance on support. Apple® macOS® 11 Big Sur Apple® macOS® 10.15 Catalina Apple® macOS® 10.14 Mojave |
|
Supported web browsers |
Google® Chrome™ version 100 or later Microsoft® Edge® version 100 or later
Apple®
Safari® 13.1
Note: In macOS, you cannot view Graphics+
graphics in the Site Management Portal UI. You use the web
browser to download the Launcher application. After you
install the Launcher application, you use the Launcher, not
the web browser, to log in to the Site Management Portal
(SMP) UI.
|
Microsoft® Edge® version 100 or later
Google®
Chrome™ version 100 or
later
Note: Metasys UI
does not support Incognito mode. To exit Incognito mode,
click or tap the X icon of the
browser window or tab and then open a new browser window or
tab. For more information on Incognito mode in Google
Chrome, click here.
Apple®
Safari® 15.0 or later
Note: Metasys UI does
not support private browsing. To exit private browsing,
click or tap Private in the browser
window.
Other web browsers, such as Mozilla® Firefox®, are not officially supported by the UI. However, the Metasys UI may appear and function appropriately in these web browsers. |
|
Supported mobile phone operating systems |
N/A |
Android phone 5.1 or later iPhone iOS 13.0 or later |
|
Supported tablet operating systems |
N/A |
Android tablet 5.1 or later iPad iOS 13.0 or later |
|
Network communication |
Ethernet network interface card 10/100/1000 Mbps |
Ethernet network interface card 10/100/1000 Mbps Follow these guidelines and recommendations:
|
|
Monitor |
1024 x 768 or higher resolution and 16-bit or higher color depth |
1024 x 768 or higher resolution and 16-bit or higher color depth Other features may require 1600 x 900 resolution. Additionally, you may need to set your monitor display at Small 100% setting (Control Panel > All Control Panel Items > Display). |