ADX with the Metasys Advanced Reporting System - Metasys - LIT-1201525 - MS-ADX50SQL2 - MS-ADX25SQL - MS-ADXS25U - MS-ADS05U - MS-ADX10SQL - MS-ADX10U - MS-ADX50U - Server - ADS Server - ADX Server - 12.0.50

Application and Data Server (ADS) and Extended Application and Data Server (ADX) Product Bulletin

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201525
Version
12.0.50
Revision date
2023-05-22
Product status
Active

The Metasys Advanced Reporting System provides historical and configuration data reporting capabilities in a UI that is separate from the Site Management Portal UI. This system allows authorized users to run reports to review the configuration and performance of the Metasys system.

The Metasys Advanced Reporting System UI allows you to run reports easily and immediately view them in a web browser.

Figure 1. Metasys Advanced Reporting System

The following reports are available for the points included in the reporting system user views:

  • Configuration Setup Review

  • System Behavior

  • Trend Summary Report — statistical calculations and Mean Kinetic Temperature (MKT)

  • Trend Detail Report — summary data

You can export a report and save it in a variety of formats, such as Microsoft Excel® or PDF, for later use.

Figure 2. Metasys Advanced Reporting System Example Report

The Metasys Advanced Reporting System is available on ADXs running SQL Server software with SQL Server Reporting Services. The Metasys Advanced Reporting System is an option during the ADX installation. Users are authorized with the Advanced Reporting option in the Security Administrator System. For details, refer to the Metasys Advanced Reporting System Help (LIT-12011312)