Metasys UI - Metasys - LIT-12011694 - MS-ADSLA5U-0 - MS-ADSLA5U-6 - Server - ADS-Lite Server - 13.0

Application and Data Server (ADS) Lite-A System Product Bulletin

Product
Building Automation Systems > Databases and Data Servers > ADS-Lite Server
Document number
LIT-12011694
Version
13.0
Revision date
2023-09-13
Product status
Active

The Metasys UI is an HTML5-compliant web interface that provides device-agnostic access to Metasys from smartphones, tablets, and computers. The Metasys UI is an intuitive interface that reduces learning time, maximizes productivity of operators, and provides a seamless user experience no matter what type of client device is used to access the system. The client device does not require any additional software installation—no Java™, Microsoft Silverlight®, Adobe®, Flash® or any other software from an online app store. The Metasys UI is included with SNE, SNC, NAE85, LCS85 series network engines, and any Metasys server: ADS, unified and split ADX, and ADS-Lite. You must license the server software to log on to the Metasys UI.