Access through the Launcher Application - Metasys - LIT-12011694 - MS-ADSLA5U-0 - MS-ADSLA5U-6 - Server - ADS-Lite Server - 13.0

Application and Data Server (ADS) Lite-A System Product Bulletin

Product
Building Automation Systems > Databases and Data Servers > ADS-Lite Server
Document number
LIT-12011694
Version
13.0
Revision date
2023-09-13
Product status
Active

Use the Launcher application to connect to the Site Management Portal UI of the ADS-Lite-A by using a desktop, laptop, or other type of computer connected to a corporate intranet, dedicated BAS, Internet, or telephone line from remote sites. Multiple users can communicate simultaneously with the server, and access is based on the authorization level assigned to individual users.

Launcher is a software application that you download when you browse to any Release 9.0 Metasys or later server or network engine on the building network. After you install the Launcher software, use it to launch the Site Management Portal UI. In addition, you can configure the Launcher to browse to any website, such as the Metasys UI . For more details, refer to the Launcher Tool Help (LIT-12011742) .