Automation Level Communication - Metasys - LIT-12011694 - MS-ADSLA5U-0 - MS-ADSLA5U-6 - Server - ADS-Lite Server - 13.0

Application and Data Server (ADS) Lite-A System Product Bulletin

Product
Building Automation Systems > Databases and Data Servers > ADS-Lite Server
Document number
LIT-12011694
Version
13.0
Revision date
2023-09-13
Product status
Active

Network engines communicate internal system data using peer-to-peer messaging over the IP Ethernet network. Each NAE45-Lite or SNE110L shares data and has access to information on the other engines connected on the network, which enables coordination and control of the entire building management system.