ADS-Lite-A concurrent users - Metasys - LIT-12011694 - MS-ADSLA5U-0 - MS-ADSLA5U-6 - Server - ADS-Lite Server - 13.0

Application and Data Server (ADS) Lite-A System Product Bulletin

Product
Building Automation Systems > Databases and Data Servers > ADS-Lite Server
Document number
LIT-12011694
Version
13.0
Revision date
2023-09-13
Product status
Active

The following table shows examples of the total number of supported users who can be simultaneously logged in to the SMP and Metasys UI.

Note: The following information provides the supported concurrent user limitations. Usage beyond the supported limitations may yield system or server performance issues.
Table 1. Examples of ADS/ADX/ADS-Lite concurrent users
ADS/ADX type Examples of ADS/ADX concurrent users
SMP UI Metasys UI

5-user ADS/ADS-Lite

0 5
2 3
5 0