The following table shows examples of the total number of supported users who can be simultaneously logged in to the SMP and Metasys UI.
Note: The following information provides the
supported concurrent user limitations. Usage beyond the supported limitations may
yield system or server performance issues.
ADS/ADX type | Examples of ADS/ADX concurrent users | |
---|---|---|
SMP UI | Metasys UI | |
5-user ADS/ADS-Lite |
0 | 5 |
2 | 3 | |
5 | 0 |