| Output Attribute | Description |
|---|---|
|
DAP-SP |
This is the discharge air static pressure setpoint (AV). It should be mapped to your discharge air static pressure setpoint in your local field controller. |
|
DAT-SP |
This is the discharge air temperature setpoint (AV). Note: This should be mapped to your discharge air temperature setpoint (DAT-SP) and not the effective discharge air temperature setpoint (EFFDAT-SP) in your local field controller.
|
|
TIMER |
Internal timer - BV false/true. |
|
TIMER-RESET |
Internal timer - BV false/true. |