Output Attributes - Metasys - LIT-12012070 - Field Device - VAV: Variable Air Volume Controller

Air Handling Unit Reset Application Note

Product
Variable Air Volume > Variable Air Volume Controls > VAV: Variable Air Volume Controller
Document type
Application Note
Document number
LIT-12012070
Revision date
2018-03-01
Table 1. Output Attributes
Output Attribute Description

DAP-SP

This is the discharge air static pressure setpoint (AV). It should be mapped to your discharge air static pressure setpoint in your local field controller.

DAT-SP

This is the discharge air temperature setpoint (AV).

Note: This should be mapped to your discharge air temperature setpoint (DAT-SP) and not the effective discharge air temperature setpoint (EFFDAT-SP) in your local field controller.

TIMER

Internal timer - BV false/true.

TIMER-RESET

Internal timer - BV false/true.