Features and Benefits - Metasys - LIT-1201848 - Software Application - Advanced Graphics Application - 10.0
Advanced Graphics Application Product Bulletin
- Product
- Building Automation Systems > Graphics and Interfaces > Advanced Graphics Application
- Document type
- Product Bulletin
- Document number
- LIT-1201848
- Version
- 10.0
- Revision date
- 2018-12-17
- Integration with the Existing Metasys System Site Management
Portal
- Provides the same binding and aliasing capabilities when creating
advanced graphics (using the Advanced Graphics Application) as when
creating graphics using the standard graphics feature and offers
consistent viewing of both types of graphics in the Metasys
system Site Management Portal.
- Dynamic Symbol Capabilities, Such as Rotate, Hide, Color Change, and
Sound
- Provide an enhanced user experience and the ability to communicate more
information in the same amount of space on the graphic.
- Stencil Library
- Provides prepackaged symbols that work in standard or dynamic mode and
keeps the additional cost in graphics development low.
- Custom Symbols and Stencils
- Provide the ability to create custom graphics in addition to using the
symbols included in the stencil library.
- Advanced Graphic Viewing in the SMP UI Framework
- Eliminates the need for separate viewing software.
- Ability to Launch Other Documents and Applications Viewable by
Browser
- Provides greater multimedia functionality, such as viewing PDFs,
spreadsheets, and video attached to graphics.