Precache Feature - Metasys - LIT-1201848 - Software Application - Advanced Graphics Application - 10.0

Advanced Graphics Application Product Bulletin

Product
Building Automation Systems > Graphics and Interfaces > Advanced Graphics Application
Document number
LIT-1201848
Version
10.0
Revision date
2018-12-17

The Precache feature of the Advanced Graphics Application improves the performance of large graphics by retrieving the values of all objects referenced in the precache definition and placing them in memory before the graphics are rendered. This feature allows object values to appear immediately when the graphics are rendered.