Graphics Viewing - Metasys - LIT-1201848 - Software Application - Advanced Graphics Application - 10.0

Advanced Graphics Application Product Bulletin

Product
Building Automation Systems > Graphics and Interfaces > Advanced Graphics Application
Document number
LIT-1201848
Version
10.0
Revision date
2018-12-17

In the SMP UI or SCT UI navigation tree, graphics created with the Advanced Graphics Application appear just like any other graphic object. When you display the advanced graphic, it appears directly in the user interface framework of the SCT (for simulating data) or the ADS/ADX (for live data and system navigation). If you view the advanced graphic in the SMP UI, you see real-time controller field point data in the graphic and are able to command and update points using the graphic.

Note: We do not recommend viewing advanced graphics in the NAE, NCE, or NIE user interfaces. Viewing advanced graphics in these device user interfaces consumes maximum flash memory of the device.