Graphics Generation Environment - Metasys - LIT-1201848 - Software Application - Advanced Graphics Application - 10.0

Advanced Graphics Application Product Bulletin

Product
Building Automation Systems > Graphics and Interfaces > Advanced Graphics Application
Document type
Product Bulletin
Document number
LIT-1201848
Version
10.0
Revision date
2018-12-17

The Advanced Graphics Application is a graphics generation add-on component to Microsoft Visio Standard or Professional 2003, 2007, or 2010 software and is used to develop dynamic graphics.

The application has graphics generation, editing, and binding features. To generate system graphics, use the symbols in the stencil library, or create your own symbols and stencils. Then, program the logic and define the graphics for the desired functionality. Bind the graphic symbols to Metasys data or other data. Figure 1 shows the Advanced Graphics Application add-on screen.