The Advanced Graphics
Application is an enhanced graphics creation
package that provides dynamic graphic
capabilities, such as animation, color changing,
and flashing, for the Metasys® system. The stencil library
component of the package contains pre-built
dynamic symbols that shorten the time spent
creating system graphics. Graphics created with
the Advanced Graphics Application appear directly
in the Metasys system Site Management
Portal (SMP) UI with real-time controller field
point data and allow building operators to command
and update points. Advanced Graphics allows users
to create a comprehensive representation of
facility support systems and provides them with
easy navigation of their Building Automation
System (BAS).
Note: Advanced Graphics are not
supported in the Metasys UI.
Figure 1. Advanced Graphics Application