Metasys UI - Metasys - LIT-12011177 - M4-ADXTK-TWR - M4-ADSTK-PC - M4-ADXTK-RCK - ADS/ADX Turnkey - 12.0

ADS/ADX Turnkey User Guide

Product
Building Automation Systems > Application Servers > ADS/ADX Turnkey
Document number
LIT-12011177
Version
12.0
Revision date
2022-05-20
The Metasys UI is an HTML5-compliant web interface that provides access to Metasys from smartphones, tablets, and computers. The Metasys UI is an intuitive interface that reduces learning time, maximizes productivity of operators, and provides a seamless user experience no matter what type of client device you use to access the system. The client device does not require any additional software installation or browser plugin. The Metasys UI is included with OAS, ADS, ADX (unified and split), and ADS-Lite.
Note: The ADS or ADX server software must be licensed before you can log on to the Metasys UI. For more information, see Licensing Metasys software on an ADS or ADX Turnkey.
Figure 1. Metasys UI