Licensing SQL Server on an ADX Turnkey - Metasys - LIT-12011177 - M4-ADXTK-TWR - M4-ADSTK-PC - M4-ADXTK-RCK - ADS/ADX Turnkey - 12.0

ADS/ADX Turnkey User Guide

Product
Building Automation Systems > Application Servers > ADS/ADX Turnkey
Document type
User Guide
Document number
LIT-12011177
Version
12.0
Revision date
2022-05-20

Procedure

  1. Open the SQL Server 2019 Installation Center.
  2. In the SQL Installation Center window, click Maintenance, and then click Edition Upgrade.
  3. On the Product Key page of the upgrade wizard, select the Enter the product key option, and then enter the product key.
  4. Step through the remaining pages of the upgrade wizard to complete the licensing process.