Launching Metasys for the first time - Metasys - LIT-12011177 - M4-ADXTK-TWR - M4-ADSTK-PC - M4-ADXTK-RCK - ADS/ADX Turnkey - 12.0

ADS/ADX Turnkey User Guide

Product
Building Automation Systems > Application Servers > ADS/ADX Turnkey
Document number
LIT-12011177
Version
12.0
Revision date
2022-05-20

About this task

As configured in the factory, the ADS and ADX Turnkey computers have an icon for Launcher on the desktop. Double-click the Launcher icon to start the application. To verify that you can access SMP or SCT, complete the following steps:

Procedure

  1. On the Launcher screen, click the SMP or SCT tab to locate the device in the profile list.
  2. Click the Launch button, or right-click the profile in the list and select Launch. The standard Metasys logon screen appears.
  3. Log on to the Metasys system.
  4. Click the X icon to close the Launcher.