Creating a database backup - Metasys - LIT-12011177 - M4-ADSTK-PC - M4-ADXTK-RCK - M4-ADXTK-TWR - ADS/ADX Turnkey - 12.0

ADS/ADX Turnkey User Guide

Brand
Metasys
Product name
ADS/ADX Turnkey
Document type
User Guide
Document number
LIT-12011177
Version
12.0
Revision date
2022-05-20
Language
English

The ADS Turnkey ships with two 500 GB hard drives in a RAID 1 configuration. The ADX Turnkey ships with six 300 GB hard drives in a RAID 5 configuration. It is essential that you create a separate backup database in the event of a dual hard drive failure. For instructions on creating a separate backup database, refer to the Metasys Database Manager Help (LIT-12011202) .