Changing the default password for the Windows administrator account - Metasys - LIT-12011177 - M4-ADSTK-PC - M4-ADXTK-RCK - M4-ADXTK-TWR - ADS/ADX Turnkey - 12.0

ADS/ADX Turnkey User Guide

Brand
Metasys
Product name
ADS/ADX Turnkey
Document type
User Guide
Document number
LIT-12011177
Version
12.0
Revision date
2022-05-20
Language
English

About this task

When you sign in to Windows for the first time, the Windows operating system prompts you to change the password for the TKAdmin account. To change the password, complete the following steps:

Procedure

  1. If you signed in to Windows for the first time, skip to Step 4.
  2. Press Ctrl+Alt+Del.
  3. Click Change a Password.
  4. On the Change a password screen, enter the current Windows administrator password in the Old password field. Enter a new strong password and confirm the password.
    Note: To identify the default Windows administrator password, refer to the documentation that ships with the Turnkey.
  5. Click the right-arrow button. The new password is saved.