Verifying that the Metasys Advanced Reporting System is working properly - Metasys - LIT-12011177 - M4-ADXTK-TWR - M4-ADSTK-PC - M4-ADXTK-RCK - ADS/ADX Turnkey - 12.0

ADS/ADX Turnkey User Guide

Product
Building Automation Systems > Application Servers > ADS/ADX Turnkey
Document number
LIT-12011177
Version
12.0
Revision date
2022-05-20

About this task

Complete this section only if you installed the Metasys Advanced Reporting System on your Turnkey.

Procedure

  1. Log on to the ADX Site Management Portal from a computer on the local network that is not running a server-class operating system.
  2. From the Tools menu, click Advanced Reporting user interface.
  3. Log on to the Metasys Advanced Reporting user interface.
  4. Verify that the user interface appears correctly and that the site and ADX have the correct name.
  5. Verify that the navigation tree that appears in the Metasys Advanced Reporting user interface matches that on the SCT/ADX .
  6. Select Alarm Definition report, and then click Run.
  7. Verify that the report window appears.
    Note: The content of the window is not important at this time.
  8. Close the report window.
  9. Select Event > Summary report, and then click Run.
  10. Verify that the report window appears.
    Note: The content of the window is not important at this time.
  11. Close the report window. The verification and rename processes are complete.