Accessing the Metasys UI - Metasys - LIT-12011177 - M4-ADXTK-TWR - M4-ADSTK-PC - M4-ADXTK-RCK - ADS/ADX Turnkey - 11.0

ADS/ADX Turnkey User Guide

Product
Building Automation Systems > Application Servers > ADS/ADX Turnkey
Document number
LIT-12011177
Version
11.0
Revision date
2021-07-20

About this task

To access the Metasys UI remotely from any client device, ensure that you have Internet, intranet, or VPN access to the ADS/ADX Turnkey, and browse to https://[IP Address]/UI, where you replace [IP Address] with the IP address, host name, or server name of your Turnkey. If you are on the Turnkey computer, you can also navigate to [IP Address]/UI or localhost/UI.

Note: Ensure that your web browser has cookies enabled before you browse to the Metasys UI.

When you browse to the Metasys UI, your web browser may display a security certificate warning. The browser displays this warning if your Metasys UI site does not have a trusted security certificate.

If you see this warning, you can browse to the Metasys UI site by doing the following:
  • For the Google® Chrome™ browser:
    1. Tap or click Advanced.
    2. Tap or click Proceed to [IP Address], where [IP Address] is the IP address, host name, or server name of the Metasys Site Director. The Metasys UI login screen appears.
  • For the Microsoft Edge® browser, tap or click Continue to this website (not recommended). The Metasys UI login screen appears.
  • For the Apple® Safari® browser, tap or click Continue in the Cannot Verify Server Identity window. The Metasys UI login screen appears.

As best practice, install a trusted security certificate. For more information about installing trusted security certificates, refer to Network and IT Guidance Technical Bulletin (LIT-12011279) and contact your IT department.

When the Metasys UI login screen appears, enter your login credentials.