Verifying the computer name - Metasys - LIT-12011177 - M4-ADXTK-TWR - M4-ADSTK-PC - M4-ADXTK-RCK - ADS/ADX Turnkey - 11.0

ADS/ADX Turnkey User Guide

Product
Building Automation Systems > Application Servers > ADS/ADX Turnkey
Document type
User Guide
Document number
LIT-12011177
Version
11.0
Revision date
2021-07-20

Before shipping an ADS/ADX Turnkey, Johnson Controls configures the Turnkey with the name that the customer supplied in the their order. You can see this custom computer name on a label affixed to the unit. After you sign in to Windows for the first time, verify that the actual computer name matches the name on the label. If the computer name does not match the name on the label, contact the Johnson Controls Field Support Center. If you need to change the name of your Turnkey before placing it into service, see Appendix: Manually changing the ADS or ADX Turnkey name and the computer name.