Signing in to Windows Server for the first time - Metasys - LIT-12011177 - M4-ADXTK-TWR - M4-ADSTK-PC - M4-ADXTK-RCK - ADS/ADX Turnkey - 11.0

ADS/ADX Turnkey User Guide

Product
Building Automation Systems > Application Servers > ADS/ADX Turnkey
Document type
User Guide
Document number
LIT-12011177
Version
11.0
Revision date
2021-07-20

Sign in to the Turnkey with the default administrator password. To identify the default administrator password, refer to the documentation that ships with the Turnkey. After you sign in for the first time, follow the on-screen instructions to change the administrator password.

Note: During Microsoft Windows Setup for your ADS/ADX Turnkey, you do not need to enter the Microsoft license product key. If you are prompted to enter a product key, click Do this later. The OS activates automatically during the initial configuration.

The Settings window for the Metasys Database Manager appears. To close this window, click OK. For more information about the Metasys Database Manager, refer to the Metasys Database Manager Help (LIT-12011202) .