Retrieving a license for SQL Server that you purchased from Johnson Controls - Metasys - LIT-12011177 - M4-ADXTK-TWR - M4-ADSTK-PC - M4-ADXTK-RCK - ADS/ADX Turnkey - 11.0
ADS/ADX Turnkey User Guide
- Product
- Building Automation Systems > Application Servers > ADS/ADX Turnkey
- Document number
- LIT-12011177
- Version
- 11.0
- Revision date
- 2021-07-20
Procedure
-
Browse to the License Portal (https://software.jci.com/licenseportal/#/login), log
on, and then click the Software tab.
-
Click the download icon for the product that includes your
purchase of SQL Server. For example, if you purchase a product that includes
both an ADX 10 user license and an SQL Server license, the product name in the
License Portal is Metasys ADX 10U W/SQL 4Core Lic
(New).
-
To download only the SQL Server files, clear the check box for
the root folder, expand the Microsoft SQL Server folder and any subfolders, and
then select the check box for the SQL Server .zip file.
-
Click Download, extract
the downloaded files, and then extract the contents of the SQL Server .zip
file.
-
Browse to the extracted files, and then open the SQL Server
license folder. The name of the SQL Server license folder is similar to
SQL 4Core Lic
(New)-MS-ADXnnSQL-0.
-
Browse through each nested subfolder until you view the
contents of the x64 folder.
-
Use a text editor, such as Notepad, to open the DefaultSetup.ini file.
-
Identify the line that begins with the text
PID=. Your product key is the code between
quotation marks on that line.