Licensing Metasys software on an ADS or ADX Turnkey - Metasys - LIT-12011177 - M4-ADXTK-TWR - M4-ADSTK-PC - M4-ADXTK-RCK - ADS/ADX Turnkey - 11.0

ADS/ADX Turnkey User Guide

Product
Building Automation Systems > Application Servers > ADS/ADX Turnkey
Document number
LIT-12011177
Version
11.0
Revision date
2021-07-20

About this task

To license an ADS/ADX Turnkey, complete the following steps. For full information about activating licenses, refer to the Starting a license activation section in the Software Manager Help (LIT-12012389). To retrieve your licenses, visit the Johnson Controls License Portal.

Procedure

  1. Open the Software Manager.
  2. In the License Inventory table, click Activate New from the Choose Action menu.
  3. Select an activation method.
  4. Depending on the activation method, enter a product key, browse to a license file, or paste in a license string.
  5. Click Activate, and then click OK.