Creating a database backup - Metasys - LIT-12011177 - M4-ADXTK-TWR - M4-ADSTK-PC - M4-ADXTK-RCK - ADS/ADX Turnkey - 11.0

ADS/ADX Turnkey User Guide

Product
Building Automation Systems > Application Servers > ADS/ADX Turnkey
Document number
LIT-12011177
Version
11.0
Revision date
2021-07-20

The ADS Turnkey ships with two 500 GB hard drives in a RAID 1 configuration. The ADX Turnkey ships with six 300 GB hard drives in a RAID 5 configuration. It is essential that you create a separate backup database in the event of a dual hard drive failure. For instructions on creating a separate backup database, refer to the Metasys Database Manager Help (LIT-12011202) .