Building Automation Systems > Application Servers > ADS/ADX Turnkey
Document type
User Guide
Document number
LIT-12011177
Version
11.0
Revision date
2021-07-20
About this task
When you sign in to
Windows for the first time, the Windows operating system prompts you to change the password
for the TKAdmin account. To change the password, complete the following steps:
Procedure
If you signed in to Windows for the first time, skip to Step 4.
Press Ctrl+Alt+Del.
Click Change a Password.
On the Change a password screen,
enter the current Windows administrator password in the Old
password field. Enter a new strong password and confirm the password.
Note: To identify the
default Windows administrator password, refer to the documentation that ships with the
Turnkey.
Click the right-arrow button. The new password is saved.