Updating devices that report to the ADS/ADX Turnkey Site Director - Metasys - LIT-12011177 - M4-ADSTK-PC - M4-ADXTK-RCK - M4-ADXTK-TWR - ADS/ADX Turnkey - 11.0

ADS/ADX Turnkey User Guide

Product
Building Automation Systems > Application Servers > ADS/ADX Turnkey
Document type
User Guide
Document number
LIT-12011177
Version
11.0
Revision date
2021-07-20

About this task

Complete the following steps in the SCT for each network engine that reports to the ADS/ADX Turnkey Site Director:

Note: If the archive contains outdated information for a network engine, perform an upload for the network engine before you complete the steps in this section. For more information, refer to the Upload section in the Metasys SCT: System Configuration Tool Help (LIT-12011964).

Procedure

  1. From the Tools menu, click Manage Archive.
  2. On the Action page, select Download To Device, and then click Next.
  3. On the Select Devices page, select the network engine to download. You can select multiple network engines.
  4. Proceed to the Site Login page, enter a username and password for the network engine, and then click Test Login. Do not select Communicate via Site Director.
  5. On the Device Pairing page, select the network engine to pair, enter login details for both the Site Director and the network engine, click Test Login to verify the login details, and then click Next.
  6. On the Summary page, click Finish.

What to do next

If the Device Pairing page displays Pairing not needed, but the network engine fails to check in with the ADS/ADX Turnkey Site Director, then you may need pair the network engine and Site Director after the download completes. For more information, see Troubleshooting.

If you are not using the Metasys Advanced Reporting System, the verification and rename processes are complete. If you are using the Metasys Advanced Reporting System, go to Verifying that the Metasys Advanced Reporting System is working properly.