Finalizing Launcher settings - Metasys - LIT-12011177 - M4-ADXTK-TWR - M4-ADSTK-PC - M4-ADXTK-RCK - ADS/ADX Turnkey - 11.0

ADS/ADX Turnkey User Guide

Product
Building Automation Systems > Application Servers > ADS/ADX Turnkey
Document number
LIT-12011177
Version
11.0
Revision date
2021-07-20

Procedure

  1. On the desktop, right-click the Metasys SCT or Metasys SMP shortcut, and then click Delete.
  2. Double-click the Launcher icon or click Programs > Johnson Controls > Launcher.
  3. In the Launcher window, click the SMP tab if you want to edit an existing SMP profile, or the SCT tab if you want to edit an existing SCT profile.
  4. Select the SMP or SCT profile that you want to edit, and then click Edit. You can also right-click the profile in the list, and then click Edit.
  5. In the New Description field, type the new name that you selected for the device.
    Note: You cannot change the IP address or host name of the device on the Edit screen. To make that change, delete, and then add the device again.
  6. Click Save.
  7. Recreate shortcuts on the desktop.
  8. Go to Uploading ADS or ADX Turnkey name changes to the SCT.