Finalizing ADS or ADX Turnkey settings - Metasys - LIT-12011177 - M4-ADXTK-TWR - M4-ADSTK-PC - M4-ADXTK-RCK - ADS/ADX Turnkey - 11.0

ADS/ADX Turnkey User Guide

Product
Building Automation Systems > Application Servers > ADS/ADX Turnkey
Document number
LIT-12011177
Version
11.0
Revision date
2021-07-20

Procedure

  1. Log on to the ADS/ADX Site Management Portal.
  2. Verify that no user views are currently open.
  3. From the View menu, click Extended Labels.
  4. Double-click the Metasys site in the All Items tree.
  5. Click Edit in the display pane.
  6. In the Name and Default ADS Repository attributes, enter the new ADS/ADX name. Note the case of each letter because the name is case-sensitive.
  7. In the Time Zone attribute, set the time zone to the correct zone.
  8. Click Save.
  9. From the Action menu, click Refresh All Tabs. The site and ADS/ADX name now match.
  10. Exit the ADS/ADX Site Management Portal.
  11. Restart the computer.
  12. Go to Finalizing Launcher settings.