Using Communication Log Files - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
13.0
Revision date
2023-10-12
Product status
Active

The remote notifications provide text-only log files to help you troubleshoot email communications issues for the ADS/ADX . The communication log files contain the most recent successful and unsuccessful messages sent by the remote notifications. If a message is unsuccessful, the log file contains a message indicating the error.

When the log file reaches its size limit, the ADS/ADX saves the log file as a backup (.bak) file and starts with an empty log file. Once that log file reaches its size limit, the ADS/ADX again saves the log file as a backup file, this time overwriting the previous backup file.

You can open and view the log files using a text editor, such as Microsoft Notepad.

For more information, see the following table.

Table 1. ADS/ADX communication log files

Description

Location of the File

Size Limit

Displays the most recent communications between the ADS/ADX, and the email recipient.

C:\ProgramData\Johnson Controls\MetasysIII

1 MB