Setting power options for the ADS/ADX network card - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
13.0
Revision date
2023-10-12
Product status
Active

Procedure

  1. In Control Panel, select System and Security, System, then click Device Manager in the left pane. If the User Account Control window appears, click Continue or Yes. The Device Manager window appears.
  2. Expand the Network Adapters item.
  3. Disable Network Interface Cards (NICs) that you do not intend to use, then install and re-enable if you need them.
  4. Right-click the network card, and click Disable device.
  5. To clear the power management, right-click the network card, and click Properties.
  6. Click the Power Management tab. Clear the option Allow the computer to turn off this device to save power.
  7. Click OK.
    Note: If there is more than one network adapter listed, repeat steps 4-6 for each adapter.
  8. Close all windows.