Configuring an ADS/ADX as Site Director if you delete the current Site Director - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
13.0
Revision date
2023-10-12
Product status
Active

If you define multiple Metasys servers (ADS/ADX devices) and you delete the ADS/ADX that is defined as the Site Director, the top Metasys server shown in the all items navigation tree of the SCT archive database automatically becomes the Site Director.

Note: The ADS-Lite cannot be the Site Director for any other ADS or ADX server.

If necessary, change the Site Director in the site object. See Configuring an ADS/ADX as Site Director.