Configuring an ADS/ADX as Site Director - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
13.0
Revision date
2023-10-12
Product status
Active

About this task

When you install the ADS/ADX, it automatically defaults to Site Director. If you need to add additional repositories, add multiple ADS/ADX devices and configure the engines to check in to one ADX. To do this set the engine repository field to ADX2.

Note: The ADS-Lite cannot be the Site Director for any other ADS or ADX server.