Trend repository optimization - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document type
Commissioning Guide
Document number
LIT-1201645
Version
13.0
Revision date
2023-10-12
Product status
Active

Optimize the required storage size of the ADS/ADX Trend repository using the following methods:

  • configure larger sample intervals for individual trends

  • determine which trends to store long-term and transfer only these samples

  • configure the trends of non-critical objects to sample on large Change-of-Value (COV) increments

In addition, optimize the network communication performance for transferring trend samples from engines devices to the ADS/ADX repository using the following methods:

  • configure the Transfer Setpoint on individual trends so they transfer their samples at intervals different from other trends

  • use the ADS Delivery Time of the network engine to transfer the samples at the time when user access to the system is minimal

Refer to the Trend Extensions topic in the Metasys SMP Help (LIT-1201793) for more information.