Three new SQL databases: MetasysValue
, MetasysFault
, and MetasysFaultTriage
were introduced at Metasys Release 11.0. To
activate the databases, license the associated Metasys features. These include Potential
Problem Areas, Fault Detection, and Fault Triage. The MetasysValue and MetasysFault
databases self-maintain and store a rolling seven days’ worth of data. These databases
are not monitored or managed by Metasys Database Manager.
A repository provides long-term storage for historical data. Typically, the ADS/ADX configured as the Site Director also provides the individual repositories for trend data, event messages, audit messages, annotations, reporting, spaces authorization, potential problem areas, fault detection, and fault triage data. Individual repositories may reside in the SQL Server database. For a split ADX, the repositories are on the database server where the SQL Server software is installed. You can install a split ADX where the database server computer stores all historical data.
The following table lists the ADS/ADX repositories, the corresponding online Metasys SMP Help (LIT-1201793) or Metasys UI Help (LIT-12011953) topic, and the corresponding file name. The next sections describe the repositories in more detail and suggest ways to optimize the repositories.
Repository |
Refer To |
Database File Name on the ADS/ADX Computer |
---|---|---|
Trends |
Trend Extensions in the Metasys SMP Help (LIT-1201793) |
JCIHistorianDB |
Audits |
Audit Trail in the Metasys SMP Help (LIT-1201793) |
JCIAuditTrails |
Events |
Alarm and Event Management in the Metasys SMP Help (LIT-1201793) |
JCIEvents |
Annotation
Note: Metasys UI
does not use this database.
|
Annotating Objects/Items in the Metasys SMP Help (LIT-1201793) |
JCIItemAnnotation |
Reporting |
Advanced Reporting in the Metasys SMP Help (LIT-1201793) |
MetasysReporting |
Metasys UI Reporting |
Reporting: Trend Widget and Custom Trend Viewer in the Metasys UI Help (LIT-12011953) |
JCIReportingDB |
Spaces Authorization |
User Authorization and Dashboard Manager in the Metasys UI Help (LIT-12011953). |
SpacesAuthorization |
Potential problem areas |
Potential problem areas section in the Metasys UI Help (LIT-12011953) |
MetasysValue |
Fault detection |
Potential problem areas section in the Metasys UI Help (LIT-12011953) |
MetasysFault |
Fault triage |
Potential problem areas section in the Metasys UI Help (LIT-12011953) |
MetasysFaultTriage |