The ADS is a scalable platform that serves multiple users and provides database software options for archiving historical data using the Microsoft SQL Server® Express software database.
The extended version of the ADS, the ADX serves a larger number of users and provides higher capacity historical data storage using the SQL Server software database. The ADX may also be configured in a split configuration, where the web/application components of the ADX reside on a dedicated web/application server and the historical databases of the ADX reside on a dedicated database server. See the following table for ADX split configuration guidelines.
Product |
Guideline |
---|---|
ADX Web/Application Server |
Must be loaded on a Windows server-class operating system . Note:
|
ADX Database Server |
Must be loaded on a Windows server-class operating system. Note: SQL Server software resides on the ADX database
server. The database server stores historical Metasys system data
and serves as a historical data repository for the web/application
server.
|
System Configuration Tool (SCT) |
Must be loaded on a third server that is separate from the ADX web/application server and ADX database server. |
For ADS/ADX hardware and software requirements, refer to the Metasys® System Configuration Guide (LIT-12011832).