Antivirus software - Metasys - LIT-1201645 - MS-ADSxxx-x - MS-ADXxxx-x - Server - ADS Server - ADX Server - 13.0

ADS/ADX Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > ADS Server
Building Automation Systems > Application Servers > ADX Server
Document number
LIT-1201645
Version
13.0
Revision date
2023-10-12
Product status
Active

To maintain the integrity of your system, run frequent virus scans of the computer running the Server. Use one of the following antivirus software programs:

  • Symantec® Endpoint Protection software Corporate Edition Version 12.x or higher.

  • McAfee® VirusScan® Enterprise version 8.8 with Patch 9 or later.

  • Windows Defender® built into Windows 11®, Windows 10®, Windows Server 2019®, Windows Server 2022® .

For more information, see Appendix: Installing antivirus software.